Smart Factory Assembly

Smart Tools and Devices

Connected devices for higher process reliability and data collection: This data-driven approach empowers you to identify bottlenecks, optimize workflows, and make informed strategic choices. 

Woman sitting on workstation with connected kolver tool to assemble something.

Imagine a scenario where your assembly line seamlessly communicates with smart tools and devices, creating a harmonized network that operates with precision. Our solution integrates these devices, ensuring that they work cohesively to eliminate errors, minimize downtime, and enhance overall efficiency. 

Advantages of Parameterized Tools: 

  • Highest possible process reliability 
  • Correct parametrization of tools according to the order 
  • Wide range of standardized plug-and-play device integrations 
  • Automation of data collection and assembly steps 
  • Possibility of integrating any smart device 
  • Faster set-up of workstations 

Connect Tools and Devices With Smart Factory Assembly 

SFA | Connect Tools & Devices with Smart Factory Assembly

Everything in one assembly system: Connect your tools and devices with our Smart Factory Assembly service.

A woman sits at the workstation and assembles something with kolver tool

Screwing and Riveting

The more assembly tools and testing equipment are connected to the system, the more you can leverage the following advantages

  • Improving process reliability through signal-controlled screwing and riveting devices 
  • Reducing the error rate thanks to the counting function of the screws/rivets 
  • Securing the process flow by releasing/locking the tools 
  • Making connection points transparent through storing process data 
  • Monitoring of the tightening process 

Bossard SmartTools

Bossard Smart Tools Series

Battery-powered screwdriving and riveting devices equipped with sensors are the first step towards digitizing your production. The tools receive information about the next work step directly from the system and return information about the last work status. Configuring the tools is simple and user-friendly. 

Get more information about Bossard SmartTools

Overlay
Bossard Smart Tools Series
Bossard Smart Tools Series with intelligent screwing and riveting tools

Kolver Tools

Kolver Straight screwdriver current controlled

Kolver is a quality European manufacturer with a wide range of corded electric screwdrivers based on different technologies. Kolver industrial electric screwdrivers with torque and angle control are well-known for their durability, superior performance, and repeatability.

Get more information about Kolver tools

Overlay
Kolver Straight screwdriver current controlled

Stahlwille Tools

Stahlwille digital smart tool

Stahlwille tools are known for precision and innovation in the world of manufacturing and maintenance.

Get more information about Stahlwille tools

Download Guidemaster Software

Overlay
Stahlwille digital smart tool
Worker Guidance with Pick-to-Light

Tools for Digital Worker Guidance

One of the biggest losses in manual production is the time spent searching. By guiding employees through the assembly process in a targeted manner, search times can be massively reduced. 

Advantages of guiding employees:

  • Increased productivity, as it is always clear where the next part is
  • Reduced assembly errors, as the risk of confusion is mitigated
  • Additional security for the assembly staff to use the correct part

Pick-by-Light Applications

One Pick-by-Light

Pick-by-light applications show the employee on an integrated light display where to pick the respective components for the next work step. The process can be acknowledged via a button, the touch function on the light, or an integrated sensor. We are happy to put together a package for your specific needs. 

  

Overlay
One Pick-by-Light

Tower System

Smart Tower with two discs

The tower turns the components in the correct order towards the assembly worker. The integrated light indicates when the component is to be removed. The pick can be acknowledged either by a confirmation button or by weight (e.g. when picking ten screws weighing ten gramms each, the system acknowledges 100 gramms of weight being removed). In addition, this system offers an inventory function that counts all components and can provide an evaluation. 

Overlay
Smart Tower with two discs

Bitcube for Screw Bits

Bitcube for Smart Assembly

In the case of screwed connections, there are often different drives in the same assembly. The bits must be changed during the assembly process. The Bitcube offers an optimal solution to simplify this process. The next work step (screwing step) is only released when the correct bit has been removed and all other bits are in the jig. This ensures that the screw drives are not damaged. 

Overlay
Bitcube for Smart Assembly

Gesture Camera Systems

A yellow and black COGNEX industrial vision sensor on a white background.

Gesture camera systems offer the possibility of following the movements of the assembly worker and projecting information onto the workplace via an attached projector. Video sequences can also be played back and the positioning of parts (or the parts themselves) can be checked for correctness (also known as shadowboard). 

Overlay
A yellow and black COGNEX industrial vision sensor on a white background.
SFA Scanner

Scanners, Sensors and Cameras

To achieve the highest possible productivity, it is important that sub-steps can be automated and inputs can be processed automatically. Smart Factory Assembly offers various possibilities. 

Advantages of automating inputs

  • Productivity is not inhibited
  • Errors are reduced to a minimum

Scanners

Scanner example

The scanner can read a large amount of information into the system with one scan. The stored logic can filter out the required information. Scanners are often used to identify components, save serial numbers or start orders. With Smart Factory Assembly, different types of scanners can be coupled. Whether via cable or radio, we integrate the scanner according to your needs. 

Overlay
Scanner example

Sensors

Close-up of a sensor, which helps to automate the assembly process

In order not to interrupt the work flow, sensors help to automate the process. The type of sensor is not important. The inputs from the sensors can be used to advance the work instruction. The values from the sensors can be stored in the system if they offer an additional benefit for the production. 

  

Overlay
Close-up of a sensor, which helps to automate the assembly process

Cameras

Smart Camera example

Cameras are used to store images or information from the image area. This information can be stored in the product file and called up at any time. Depending on your needs, there are different camera systems that can be integrated. We are happy to advise you on the best option for your specific application. 

Overlay
Smart Camera example
Three engineers collaborating on various tests in a well-equipped laboratory, with a clear view of both the team and the testing equipment.

Automatic Measuring and Control

In addition to automating inputs via scanners, sensors or cameras, measuring outcomes and controlling steps can also be automated. Our Smart Assembly service offers you various possibilities to do so, from smart weighing systems to identification systems.

Advantages of automating measuring and control:

  • Productivity is not inhibited
  • Errors are reduced to a minimum
  • All data are stored in a database

Weighing Systems

Digital scale with a stainless steel platform and a separate LCD display showing numbers, surrounded by control buttons.

Measuring weight can be helpful in a production in different steps. Whether weighing the package contents at the end of a line to ensure that nothing has been forgotten or to verify the number of screws to be used. We are pleased to help you with the design of such systems.

Overlay
Digital scale with a stainless steel platform and a separate LCD display showing numbers, surrounded by control buttons.

Electrical Tests

Electrical Tests

Electrical components are subjected to a functional test at the end of production. In some cases, it is necessary to measure whether current is running through the cables. With a test program, this process can also be automated and controlled by a control system. We gladly advise you on the configuration of tests in this area. 

Overlay
Electrical Tests

Identification Systems

Identification Systems

For certain products it may be useful to identify employees who manufacture the product. For example, if a training course has to be compared (welding, screwing, etc.) or certain checks have to be made with a 4-eyes principle. With an identification system, these parameters can be checked and the information stored. 

Overlay
Identification Systems
White robotic arm with blue accents attached to a wheeled base.

Integrating Robots and Cobots

For complex tasks that require high accuracy or are very monotonous, the support of collaborative robots (Cobots) can relieve the workload of your employees and increase productivity. Cobots are controlled by the system, similar to the way a screwdriver works. The programs are taught and programmed via the robot’s software. The Cobot receives the signal for the work to be carried out in the corresponding work step. We are happy to support you in integrating Cobots into your Smart Assembly system.

Advantages of using collaborative robots:

  • Increasing productivity through parallel working
  • Reducing errors to a minimum
  • Process-safe attitude of the accuracy
  • Avoiding monotony for employees

Are You Ready to Go?

Learn more about assembly digitalization. Consult our experts today.

Two men at a screen point to the elam solutions shown

Contact Us for a Free Demo

Please complete the form. *fields are required.

Related Topics You Might Be Interested In