Since Bossard SmartBin was first introduced in 1998, it has helped many of our customers to achieve greater efficiency in procurement.
SmartBin – automatic intelligence
Bossard SmartBin is used in many different ways
![Bossard SmarBin Logistic System](https://media.bossard.com/-/media/bossard-group/website/images/logistics/smart-bin-flex-large.jpg?h=768&w=1024&la=en&hash=AA35E6DF0BD0935CDBA0D69228702CF4)
SmartBin flex
The latest invention makes logistics even more independent, flexible, and still fully automated. SmartBin flex can be placed wherever needed and doesn't even need a power connection to support lean manufacturing. The signals are transmitted wirelessly. SmartBin flex can be installed on a work cell or directly at the assembly line. This eliminates waiting times and goods movements as the material is supplied directly to the point of use.
![Bossard SmarBin Logistic System](https://media.bossard.com/-/media/bossard-group/website/images/logistics/smart-bin-mobile-large.jpg?h=1382&w=922&la=en&hash=BBD49957C4878FB716C78B8CFF0683DB)
SmartBin mobile
An ideal solution when assembly processes involve the integration of large objects or changing working environments. Mobile trolleys are equipped with SmartBin, wireless communication, and powered by a battery. You take along the C-parts to the point of use.
![Bossard SmarBin Logistic System](https://media.bossard.com/-/media/bossard-group/website/images/logistics/smart-bin-classsic-large.jpg?h=768&w=1024&la=en&hash=A601DDDC88766D89B0F3B6FDB51ACBC0)
SmartBin classic
The classic version of SmartBin is used for Kanban pools.
It supports centralized and decentralized Kanban pools. SmartBin is able to manage small parts of a few grammes per bin or high volumes and large parts of up to 1,000 kg per palette.
Watch how SmartBin works